Hi sebastanst,To generate an interrupt when receiving message to the mailbox you just need to add ST25DV_GPO_RFPUTMSG_MASK to the configIT parameter (or replace ST25DV_GPO_FIELDCHANGE_MASK with it). But to generate the interrupt from the GPO, the fas...
Hi Nishi,Do you have any data after the CCFile?NfcType5_NDEFDetection is looking for TLV data after the CCFILE and return an error if it doesn't find it.Kind Regards.
Hi Ulysses,Thank you to pinpoint that smart cards / java cards are ISO/IEC 14443 interfaces, because ST25 tags with Energy Harvesting feature are only on ISO 15693 standard.Kind Regards.
Hi praveenbm5,I cannot answer for the ST33 Secure MCU and you should contact the local sales for that product to get more information as this is not a public product.Regarding the ePaper, the power required when updating the screen can be provided by...
Hi eagles64,Can I put multiple function records in one NDEF file?For example, I just want to connect uri link with one NDEF file and also wifi connection at the same time.Is it possible? Yes it's possible, 1 NDEF file can include multiple records. If...