User Activity

Moved from MPUs forum.Hi, i must Use a Single Port Gigabit Ethernet PHY  that have a RGMII Gigabit Interface to connect a RMII 10/100 MbitEthernet MAC interface of the STM32H563VI MCU. Do you think it is possible to connect a Gigabit PHY chip to the ...
Hi,I'm start to Develop a New Project system with eLearning programs. I would like to mainly use a single development tool: STM32 CubeIDE with an .ioc configure and C Firmware Source and Include code... 1) Is it possible to use only the CubeIDE alm...
Hy, i must Drive the Clock PIN of the L6208 with the Timer_1-CH1 pin41 or Timer2-CH2 pin42,it's the same for me (micro STM32F100). There is a routine firmware, a library or a C function, with the configuration and control mode of the Timer_1 to gener...
Hello, were can i find the Description and the Firmware library with all the complete funcionsof the ​powerSTEP01 microstepping controllerI want control the powerSTEP01 with STM32 F4 microcontroller via SPI and I/O controli don't find the complete fi...
Kudos from