Question
Stepper Motor Drive L6208 With STM32F100RBT6B
Hy, i must Drive the Clock PIN of the L6208 with the Timer_1-CH1 pin41 or Timer2-CH2 pin42,
it's the same for me (micro STM32F100). There is a routine firmware, a library or a C function, with the configuration and control mode of the Timer_1 to generate the constant duty cycle signal about 50% and variable frequency for example from 200 Hz to 4000 Hz to drive the clock pin of the L6208 ??
Thank you very much