User Activity

I would like to use the mbedTLS version 2.28.2.v2 on the secure boot for stm32h743ii controller. I have downloaded SBSFU v2.6.2 and Built the secure boot binary on top of the example project from H753 2_images_OSC folder. Secure boot is running the t...
I am using the SBSFU STM32CubeExpansion_SBSFU_V2.6.2 version for my custom board STM32H743VI controller. I have ported the STM32H7B3I-DK project for H743 controller for COM port and changed the crypto scheme to SECBOOT_ECCDSA_WITHOUT_ENCRYPT_SHA256. ...
I have flashed the SBSFU application with write protection enabled for flash address 0x08000000. After that, I am unable to erase using jlink commander.exe as well as by IAR->project->Download->erase.STM32H743 has SWD interface and i am using jlink ...
Kudos given to