User Activity

Hi ST CommunityI'm working on a BLE Beacon application. There is a device which is beaconing every second. Goal is to scan for these beacons and update to gateway.  Using this function 'aci_gap_start_general_discovery_proc' to scan for the beaconing ...
Hi community,I have an application to sample the ADC and go to sleep(STOP2) mode. From the RM0434 got to know that cannot use the ADC/DMA interrupt as a wakeup source to get the ADC converted valuesSo I went with the Polling approach as shown in the ...
Hi ST Community Is it possible to use the ADC polling/DMA/IT in STOP2 mode. The application is to develop a low power platform for ADC sampling and go back to sleep. After a certain period send this data over BLE.
Hey,I'm working on custom BLE Central and Peripheral project to make connection and send some sensor data over BLE. For this I'm referring to BLE p2pServer and p2pClient along with p2pRouter example projects. I'm able to make a connection with the se...
Hello,I'm using a custom board which has STM32WB55 as the MCU. For the application, requires the MCU in sleep mode. The chosen sleep mode is STOP2. I referred the example project 'PWR_STOP2_RTC' which is available for the p-nucleo board and tried to ...
Kudos from
Kudos given to