cancel
Showing results for 
Search instead for 
Did you mean: 

ADC in STOP2 mode

ABN
Associate III

Hi ST Community

 

Is it possible to use the ADC polling/DMA/IT in STOP2 mode. The application is to develop a low power platform for ADC sampling and go back to sleep. After a certain period send this data over BLE.

1 ACCEPTED SOLUTION

Accepted Solutions

For the first and a second question, i think t

You can follow the same steps as on this example.

Best Regards 

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
STTwo-32
ST Employee

Hello @ABN 

As you can see on the table table 25 of the RM0434, the ADC can work only in RUN, SLEEP, Low Power run and Low Power Sleep modes:

Screenshot_2024-08-20-06-31-06-17_e2d5b3f32b79de1d45acd1fad96fbb0f.jpg

Best Regards

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

ABN
Associate III

Hi @STTwo-32 

Thanks for sharing the table. I have couple more questions
1. Any necessary steps to be taken to put ADC block in low power mode

2. After waking up from STOP2 mode, any re-initialization of ADC to be done so that ADC can be used in RUN mode?

For the first and a second question, i think t

You can follow the same steps as on this example.

Best Regards 

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

@STTwo-32 

I went through the example. But I was not able to see the IOC configuration and the driver files. Instead of the approach given in the example, I used ADC Polling method

ABN_0-1724225756624.png

In this approach I'm getting HAL_ERROR in the HAL_ADC_PollForConversion

The example is not based on the CubeMX. So, there is not a .ioc file for this project. For the Error, this is not on the same context of this post. I suggest you create a new post (after selecting a best answer for this one) on the Embedded Software forum. You should find there the help you need.

Best Regards.

STwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.