Windows 10 64bit - STM32CubeMX 6.0.1 - STM32H7B3LIHxQ MCUAttempting to generate a fresh project and get the below error. Any thoughts on how to resolve the issue? project file attached. Thanks!
Posted on October 24, 2017 at 02:57Hi all,I'm somewhat new to the micro world of development. I am trying to create a fairly large object in the SRAM on the F429Disco.I am using the FMC_SDRAM example provided by ST. It compiles and run fine Out of t...
Posted on February 08, 2016 at 21:56
Hi,
I'm using a STM32F429 disco board. I used the CubeMX to gen my HAL. Everything works pretty great, except for after a while my CAN IT stops firing.
Here is my code below. In the HAL_CAN_RxCp...
Posted on February 04, 2016 at 16:20
Used the STMCubeMX to generate the code. STM32F429I disco board, CAN running at 500k.
I added a very simple to the loop,
hcan1.pTxMsg->StdId = 0x11;
hcan1.pTxMsg->ExtId = 0x01;
hcan1.pTxMsg-...
Posted on February 04, 2014 at 22:53
Gents (and maybe Ladies),
My goal is to wait until a certain amount of data has been received. I have setup an interrupt (Can Bus) and when it is triggered it stuffs the message into an Array. I'm usin...
Hi,I removed the JDK v13.0.1, restarted, deleted all non necessary files in that directory and project generation is now successful! Thank you for your help!Matt
Hi @Aymen CHAKROUN I removed all java and installed 64 bit java version "1.8.0_261"Java(TM) SE Runtime Environment (build 1.8.0_261-b12)Java HotSpot(TM) 64-Bit Server VM (build 25.261-b12, mixed mode)I am running the .exe file (shortcut). I have tri...
Hi Aymen,java version "1.8.0_261"Java(TM) SE Runtime Environment (build 1.8.0_261-b12)Java HotSpot(TM) Client VM (build 25.261-b12, mixed mode, sharing)Thanks!Matt
Posted on October 24, 2017 at 03:40Thank you for responding! Seems like I need to update the linker script or add in some flags to the linker so it is aware of the extra SDRAM