User Activity

Hey!When I use images in TouchGFX, the color sequence seems different than in regular widgets. It only appears when images are stored on external flash (QSPI flash in my case), images stored on internal flash are fine.Below is an example: the top 3 s...
Hey!I'm trying to use ST-LINK/V2-1 from Nucleo to program and debug my board. I removed the jumpers from CN2 and connected CN4 to my board according to the manual:Problem occurs when I tie NRST of the CN4 to the STM32 on my board - in this case  "DEV...
Hey!I initialized the TIM1 peripheral to output an complementary PWN signal on channel 2 (PB14) and tested it with an oscilloscope. Signal is present, everything's fine.Then after initialization of the SPI2 peripheral (PB13 & PB15) PWM signal is no l...
I'm completely lost in ADC working modes. And it happens EACH time I start a new project with internal ADC. So it ends up taking a lot of time to get the ADC do what I want.I need the following behaviour: 2 channels of single adc runs forever.By my r...
Kudos from
Kudos given to