Hi. Since the last update I can no longer create a new workspace.Any help is appreciated.OpenSUSE Linux Thumbleweed here.Best regards,Marcelo..metadata/.ide.log:2023-04-30 16:42:26,518 [INFO] Activator:176 -
2023-04-30 16:42:26,520 [INFO] Activa...
Hi @heveskar ,You are absolutely right, the system memory address is wrong in the revision of AN2606 that is shown in the previous reply. In AN2606 revision 62 page 269, section 53.1, we can see the same table, with the corrected address: System memo...
Hi,Same problem here, using a Nucleo-H745ZI-Q.I don't know if it helps you guys, but here is the diff that was applied to my IOC file. It does not allow me to generate code.Regards,Marcelo.
Hi,After some debugging, I found that there is a parameter called SDMMC clock divide factor that defaults to zero. The path to it is Connectivity -> SDMMC1 -> Configuration -> Parameter Settings -> SDMMC clock divide factor. I have set it to 1, which...
It does not work for me too.My experience is the following: HAL_SD_Init() is being called twice. The first time is from MX_SDMMC1_SD_Init(). This time, SD_WideBus_Enable() works fine and returns HAL_SD_ERROR_NONE:Thread #1 [main] 1 [core: 0] (Suspend...