User Activity

Hi, I'm hosting a VL53L8CX with a STM32F4, 48-pin instead of the 64-pin on your eval board. There's a 5" flex cable between processor and L8. The vl53l8cx_init() function was failing. Slowing the SPI baud didn't help. Increasing wait time on line 276...
Hello @John E KVAM ,Table 14 in the datasheet shows power consumption in Autonomous as going as low as 4.5 mW, but is this only the AVDD power? or total device power? Because I do measure low power draw at those levels, but only on the AVDD pin (and ...
The eval board for the VL53L5 has a GUI that displays all of the zones. Is there a similar GUI for the 53L8 eval board? I don't see one listed on the Tools and Software tab for the eval board. Or is there a way to make the L5
When VL53L5CX Time-of-Flight sensor is in threshold detect mode, will it trigger only on what would be a Status 5 valid distance? Thanks! -Doug
I'm looking at the I2C spew from a VL53L5C, and it appears to be values for each of 64 zones. Data for a particular zone starts with Z_______ where the blank is the zone number. But instead of starting with Z 0 to Z3F (0 to 64) it goes from ZFFFFFFC ...
Kudos from
Kudos given to