User Activity

Hi!STM32CubeMX generated an incorrect linker file, and I can't build the project with cmake.Example project attached to the post.cmake version - 3.28.1STM32CubeMX version 6.12.1
Hello ST community.I am use NUCLEO-G474RE, wanted to set up HRTIM in push pull mode with dead time. I select the set and reset sources for outputs TA1 and TA2 period event and compare 1 event. But when i turn on dead time, TA2 setting is considere...
Hello ST community,I am use NUCLEO-G474RE, wanted to set up SYNCOUT for HRTIM. You can see the synchro configuration below:Timer A is running, PWM is generated, but nothing happens to SYNCOUT. I start looking at hrtim initialization and notice that t...
Kudos from
Kudos given to