cancel
Showing results for 
Search instead for 
Did you mean: 

SPL Initialize Error on DDR Ram speed

gianlucarenzi
Associate III

Hello,

I am trying to bring up a custom board based on the STM32MP157D MPU via SDCard.

I am using u-boot 2022-01-rc3 as bootloader and the boot is using SPL (I have an SDCard with a GPT Partition table with fsbl1, fsbl2 and ssbl named partitions).

This is the 2nd time I am using this u-boot to bring up a custom STM32MP15x board.

The first time was using a STM32MP151a and I needed to activate the clock tree for the USART1 and modified the low level setup in the stm32mp1_clk source code to enable the USART1 clocks and to activate the serial port #1 to have the SPL ready to print as soon it starts.

But now, something goes wrong. I am using a DDR3 layout as the ED1 evaluation kit as 2x4GB (2x16 bit) 533Mhz DDR RAM. Using the same clk initialization stuff in the ddr3-1066-888-bin-g-2x4gb-533mhz device tree file, and the rcc configuration as follow:

&rcc {
	status = "okay";
	st,clksrc = <
		CLK_MPU_PLL1P
		CLK_AXI_PLL2P
		CLK_MCU_PLL3P
		CLK_PLL12_HSE
		CLK_PLL3_HSE
		CLK_PLL4_HSE
		CLK_RTC_LSE
		CLK_MCO1_DISABLED
		CLK_MCO2_DISABLED
	>;
 
	st,clkdiv = <
		1 /*MPU*/
		0 /*AXI*/
		0 /*MCU*/
		1 /*APB1*/
		1 /*APB2*/
		1 /*APB3*/
		1 /*APB4*/
		2 /*APB5*/
		23 /*RTC*/
		0 /*MCO1*/
		0 /*MCO2*/
	>;
 
	st,pkcs = <
		CLK_CKPER_HSE
		CLK_FMC_ACLK
		CLK_QSPI_ACLK
		CLK_ETH_DISABLED
		CLK_SDMMC12_PLL4P
		CLK_DSI_DSIPLL
		CLK_STGEN_HSE
		CLK_USBPHY_HSE
		CLK_SPI2S1_PLL3Q
		CLK_SPI2S23_PLL3Q
		CLK_SPI45_HSI
		CLK_SPI6_HSI
		CLK_I2C46_HSI
		CLK_SDMMC3_PLL4P
		CLK_USBO_USBPHY
		CLK_ADC_CKPER
		CLK_CEC_LSE
		CLK_I2C12_HSI
		CLK_I2C35_HSI
		CLK_UART1_HSI
		CLK_UART24_HSI
		CLK_UART35_HSI
		CLK_UART6_HSI
		CLK_UART78_HSI
		CLK_SPDIF_PLL4P
		CLK_FDCAN_PLL4R
		CLK_SAI1_PLL3Q
		CLK_SAI2_PLL3Q
		CLK_SAI3_PLL3Q
		CLK_SAI4_PLL3Q
		CLK_RNG1_LSI
		CLK_RNG2_LSI
		CLK_LPTIM1_PCLK1
		CLK_LPTIM23_PCLK3
		CLK_LPTIM45_LSE
	>;
 
	/* VCO = 1066.0 MHz => P = 266 (AXI), Q = 533 (GPU), R = 533 (DDR) */
	pll2: st,pll@1 {
		compatible = "st,stm32mp1-pll";
		reg = <1>;
		cfg = < 2 65 1 0 0 PQR(1,1,1) >;
		frac = < 0x1400 >;
		u-boot,dm-pre-reloc;
	};
 
	/* VCO = 417.8 MHz => P = 209, Q = 24, R = 11 */
	pll3: st,pll@2 {
		compatible = "st,stm32mp1-pll";
		reg = <2>;
		cfg = < 1 33 1 16 36 PQR(1,1,1) >;
		frac = < 0x1a04 >;
		u-boot,dm-pre-reloc;
	};
 
	/* VCO = 594.0 MHz => P = 99, Q = 74, R = 74 */
	pll4: st,pll@3 {
		compatible = "st,stm32mp1-pll";
		reg = <3>;
		cfg = < 3 98 5 7 7 PQR(1,1,1) >;
		u-boot,dm-pre-reloc;
	};
};

it fails with:

U-Boot SPL 2022.01-rc3 (Aug 04 2022 - 17:01:02 +0200)
RAM: EK470 DDR3-DDR3L 32bits 533000kHz
stm32mp1_clk rcc@50000000: stm32mp1_clk_disable: id clock 228 has been disabled
stm32mp1_clk rcc@50000000: stm32mp1_clk_enable: id clock 220 has been enabled
stm32mp1_clk rcc@50000000: stm32mp1_clk_enable: id clock 222 has been enabled
stm32mp1_clk rcc@50000000: stm32mp1_clk_enable: id clock 226 has been enabled
stm32mp1_clk rcc@50000000: stm32mp1_clk_enable: id clock 229 has been enabled
stm32mp1_clk rcc@50000000: stm32mp1_clk_enable: id clock 224 has been enabled
id=15 clock = 1fc4ef40 : 533000 kHz
stm32mp1_clk rcc@50000000: computed rate for id clock 224 is 533000000 (parent is PLL2_R)
stm32mp1_clk rcc@50000000: stm32mp1_clk_enable: id clock 228 has been enabled
get_ram_size(c0000000, 40000000)
info.size: 4
DDR invalid size : 0x4, expected 0x40000000
DRAM init failed: -22
### ERROR ### Please RESET the board ###

I suppose the ddr3 setup file in u-boot dts is using the right setup of memory (as the ed1 board I suppose it is working fine), so I cannot understand why the get_ram_size() function returns a single 32 bit (4 bytes) size.

Can help you out to jump over this issue?

Can be a wrong voltage on the DRAM chips?

Regards,

Gianluca

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
gianlucarenzi
Associate III

as far as I know the vdd_ddr: buck2 is 1350000 microvolts 1.35V in the device-tree configuration of the STPMIC2APQR.

gianlucarenzi
Associate III

Just checked. VDD_DDR (despite the Buck2In is present (5VCC)) is 0V. This should explain the wrong DDR Calculation. Maybe it needs a working SDRAM chip ofcourse.

Now the REGULATORS is defined in the config:

CONFIG_PINCONF=y
# CONFIG_SPL_PINCTRL_FULL is not set
CONFIG_PINCTRL_STMFX=y
CONFIG_DM_PMIC=y
# CONFIG_SPL_PMIC_CHILDREN is not set
CONFIG_PMIC_STPMIC1=y
CONFIG_DM_REGULATOR=y
CONFIG_DM_REGULATOR_FIXED=y
CONFIG_DM_REGULATOR_GPIO=y
CONFIG_DM_REGULATOR_STM32_VREFBUF=y
CONFIG_DM_REGULATOR_STPMIC1=y

as well as the i2c4 setup (pinmux and i2c core) in the device tree:

&pinctrl_z {
	u-boot,dm-pre-reloc;
 
	i2c4_pins_z_mx: i2c4_mx-0 {
		pins {
			pinmux = <STM32_PINMUX('Z', 4, AF6)>, /* I2C4_SCL */
					 <STM32_PINMUX('Z', 5, AF6)>; /* I2C4_SDA */
			bias-disable;
			drive-open-drain;
			slew-rate = <0>;
		};
	};
 
	i2c4_sleep_pins_z_mx: i2c4_sleep_mx-0 {
		pins {
			pinmux = <STM32_PINMUX('Z', 4, ANALOG)>, /* I2C4_SCL */
					 <STM32_PINMUX('Z', 5, ANALOG)>; /* I2C4_SDA */
		};
	};

The same is applied to the i2c4 bus controller:

&i2c4 {
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&i2c4_pins_z_mx>;
	pinctrl-1 = <&i2c4_sleep_pins_z_mx>;
	i2c-scl-rising-time-ns = <185>;
	i2c-scl-falling-time-ns = <20>;
	clock-frequency = <100000>;
	status = "okay";
	/* spare dmas for other usage */
	/delete-property/dmas;
	/delete-property/dma-names;
 
	pmic: stpmic@33 {
		compatible = "st,stpmic1";
		reg = <0x33>;
		interrupts-extended = <&gpioa 0 IRQ_TYPE_EDGE_FALLING>;
		interrupt-controller;
		#interrupt-cells = <2>;
		status = "okay";
 
		regulators {
			compatible = "st,stpmic1-regulators";
			buck1-supply = <&vin>;
			buck2-supply = <&vin>;
			buck3-supply = <&vin>;
			buck4-supply = <&vin>;
			ldo1-supply = <&v3v3>;
			ldo2-supply = <&vin>;
			ldo3-supply = <&vdd_ddr>;
			ldo4-supply = <&vin>;
			ldo5-supply = <&vin>;
			ldo6-supply = <&v3v3>;
			vref_ddr-supply = <&vin>;
			boost-supply = <&vin>;
			pwr_sw1-supply = <&bst_out>;
			pwr_sw2-supply = <&bst_out>;
 
			vddcore: buck1 {
				regulator-name = "vddcore";
				regulator-min-microvolt = <1200000>;
				regulator-max-microvolt = <1350000>;
				regulator-always-on;
				regulator-initial-mode = <0>;
				regulator-over-current-protection;
			};
 
			vdd_ddr: buck2 {
				regulator-name = "vdd_ddr";
				regulator-min-microvolt = <1350000>;
				regulator-max-microvolt = <1350000>;
				regulator-always-on;
				regulator-initial-mode = <0>;
				regulator-over-current-protection;
			};
 
			vdd: buck3 {
				regulator-name = "vdd";
				regulator-min-microvolt = <3300000>;
				regulator-max-microvolt = <3300000>;
				regulator-always-on;
				st,mask-reset;
				regulator-initial-mode = <0>;
				regulator-over-current-protection;
			};
 
			v3v3: buck4 {
				regulator-name = "v3v3";
				regulator-min-microvolt = <3300000>;
				regulator-max-microvolt = <3300000>;
				regulator-always-on;
				regulator-over-current-protection;
				regulator-initial-mode = <0>;
			};
 
			vtt_ddr: ldo3 {
				regulator-name = "vtt_ddr";
				regulator-min-microvolt = <1800000>;
				regulator-max-microvolt = <1800000>;
				regulator-always-on;
				regulator-over-current-protection;
			};
 
			vdd_usb: ldo4 {
				regulator-name = "vdd_usb";
				interrupts = <IT_CURLIM_LDO4 0>;
			};
 
			vdda: ldo5 {
				regulator-name = "vdda";
				regulator-min-microvolt = <2900000>;
				regulator-max-microvolt = <2900000>;
				interrupts = <IT_CURLIM_LDO5 0>;
				regulator-boot-on;
			};
 
			vref_ddr: vref_ddr {
				regulator-name = "vref_ddr";
				regulator-always-on;
			};
 
			 bst_out: boost {
				regulator-name = "bst_out";
				interrupts = <IT_OCP_BOOST 0>;
			 };
 
			vbus_otg: pwr_sw1 {
				regulator-name = "vbus_otg";
				interrupts = <IT_OCP_OTG 0>;
			 };
 
			 vbus_sw: pwr_sw2 {
				regulator-name = "vbus_sw";
				interrupts = <IT_OCP_SWOUT 0>;
				regulator-active-discharge = <1>;
			 };
		};
 
		watchdog {
			compatible = "st,stpmic1-wdt";
			status = "disabled";
		};
	};
};

And, of course, the &i2c4 used in SPL and is enabled with: &i2c4{ u-boot,dm-pre-reloc; status="okay"; } as well as the &pinctrl_z { u-boot,dm-pre-reloc; status = "okay"; }

Even the pmic node is enabled in the SPL section with: &pmic { u-boot,dm-pre-reloc; status = "okay"; }

Is there a way to check (easely) with a scope, if the SPL is using the spl pmic driver *BEFORE* checking the RAM controller. It should be called as soon as possible during boot-up.

Do you agree with me?

Regards,

Gianluca

Olivier GALLIEN
ST Employee

Hi @gianlucarenzi​ ,

I read :

"u-boot 2022-01-rc3 as bootloader and the boot is using SPL"

Likely Vanilla U-boot version not yet integrated and ST no more support SPL for MP1.

I recommend you to use an OpenSTLinux delivery to get better support.

STM32 MPU OpenSTLinux release note - v4.0.0 - stm32mpu

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.