cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F439 / SDIO / FatFS - microSD card problem

florian.morsch
Associate II

Hello,

i have a strange problem when i try to work with a FatFS on SD cards with SDIO.

MCU is a STM32F439ZI, SDIO 4 wire for SD cards, FatFS for SD cards (used CubeMX 5.1.0 to create the base code, working with Atollic TrueSTUDIO 9.0.1)

I have working code for a 4 GB microSD card, initialisation, mount, open, read/write, all works fine.

If i use a 2 GB or 8 GB microSD card i can initialize and mount (FR_OK), but when i try to open a file i get FR_NO_FILESYSTEM as result. So i implemented a check for FR_NO_FILESYSTEM and call f_mkfs, this runs fine (FR_OK), i mount the card (FR_OK) and when i try to open a file -> FR_NO_FILESYSTEM (when one operation before the f_mkfs gave FR_OK back).

When i format the card at the PC in different ways and format types (SD card formater, Windows formater, EaseUS Partition Master /// FAT, FAT32, exFAT) i still get the same FR_NO_FILESYSTEM error for the 2 GB and 8 GB microSD, while the 4 GB microSD works perfectly fine with the exact same code.

Has anyone a clue what could be the problem here?

Best regards,

Florian

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Clive1 (HNL)
Senior II

There are very few occasions where f_mkfs() is appropriate.

FR_NO_FILESYSTEM is usually an issue with reading the media properly. FATFS comes up with this after reading one or two sectors, nominally MBR and BPB.

I would tend to instrument DISKIO layer so that it dumps the initial sectors, prints the blocks/counts for read/write requests and reports read/write disk errors.