2021-02-15 02:14 AM
Hello,
Is there any ressource describing the consumption during 10Hz Low-power mode ?
On my side I think I can see little peaks each 100ms then one litle larger peak each 2 seconds.
In advance thanks
Solved! Go to Solution.
2021-02-19 08:19 AM
At the moment I just use the H3LIS331DL.
And my problem was finally the "internal pull-up on SDO" that drain about 70uA.
Looking at the datasheet this pull-up does not seem desactivable . Please confirm me.
But in a future we may use LISDE12TR and eventually in conjunction with H3LIS331DL... so in that case the "Desactivable pull-up" on LIS2DETR will be the solution. OK.
So, if you want the topic can now be closed.
Thanks for these exchanges.
2021-02-22 07:28 AM
Hi @PGoud ,
you're welcome.
>> Looking at the datasheet this pull-up does not seem de-activable. Please confirm me.
You are right, the pull-up is not de-activable from the standard configuration register. As an alternative, you could try with the 90h in CTRL_REG0 (1Eh) for the H3LIS331DL too, but this is a reserved register and should not be modified... a power off-on of the device will restore the factory calibration data.
-Eleon