User Activity

I conducted some test in case the option bytes in the STM32L474 (Nucleo 64 board) are set incorrectly for my application. Note HAL is not used (it's a strict bare metal application since this is a home experiment to reduce power consumption to the ba...
The reference manual:Present HAL implementation uses division of 1 if the selected division is unknown: the red marked source does not match the RM?
The following project is imported in the latest Cube IDE (see below for version info) in an empty, new created workspace: When the IOC file is opened / code is generated, the following pop up appears (this is also the case when importing the example...
I'm trying to use X-NUCLEO-IDB05A2 on an Nucleo64 STM32L476 board. I want is to initialize the IDB05A2 and pair it with smartphone(s) to detect if any of these paired phone(s) is in range or not (so the phone(s) should acts as paired beacon(s) / ther...
Cube IDE 1.12.0 Build 14980_2023_03_01_1550OS: Windows 11 Pro 22H2 Build 22621.1413Project using STM32L476 Nucleo board; low level only (no HAL used at all)I've build my project IOC file using the previous version of Cube. When I open it, I have 3 op...
Kudos from