User Activity

We're looking to replace our F105 processors in the next generation of a an automotive application.We want more flash,2 I2c ports2 SPI ports3 UARTspreferably 4 CAN ports, but atleast 3, 2 of the CAN ports should support CAN-FDand more hardware securi...
We're investigating replacing some STM32F105 processors with STM32F107 on a short time frame.The datasheet footnote says "SPI2/I2S2 and I2C2 are not available when the Ethernet is being used." Does that mean that I2C2 is never available or that you h...
I'm trying to generate a 2 second break from USART1 on a STM32F105. It's needed for a custom protocol running on top of LIN: the TX line must be driven low for 2 seconds.UARTs like 8250 and 16550 have a Set Break Enable Bit (SBE) in their Line Contro...
Kudos from
Kudos given to