I have a node connected to a gateway and a chirpstack server. I decided I want to understand a few topics. So I went into the above file and changed the EUI from a working 80,00,00,00,00,00,00,06 to below. #define LORAWAN_JOIN_EUI ...
I have the above subject powered with 24V, 3A power supply. The motor is not loaded. I keep having issues trying to write to the device. How do I get this warning to not appear and why is it appearing?My second question is when I do BLDC stuff wit...
Hello ....I have an apk that seems to lose comms with a server. We have not been able to make it periodic or obvious as to the reason. We would like the server to timeout after 30 seconds of not receiving read/write rqsts from the client and force ...
Good afternoon....I have a known working board with an STM32WB5MMGH6TR (server). I am using an apk on a google pixel 6a. The application scans for the device and if not found has a re-scan button that user can hit to try and connect (I am not the w...
Using a Nucleo-F072RB. I am trying to get the output of CC1 to go low after the CPU does something. Everything is working as expected except I cannot get the line to go low. I have tried both variants of the CC1P bit and neither seems to work. I ...
Yes but the question still remains....with respect to firmware / CubeMX / STM32WB55 and BLE in general....Does it stop advertising at some point and if so do you kick it to restart it OR is there some combination of settings in Configuration I should...
Thank you very much for all the help! After taking your information and going back a few steps then rebuilding from scratch up I got something that works pretty well.Your MOE and CC1E bits were important.Clock frequency played a role as when I moved...
Ok....so firstly (THANK YOU for your patience!!!)....I took CubeMX and set Channel 1 as Output Compare CH1..ie AF bit gets set now...It seems the code does not touch the CCER / BDTR registers so I did this manually in the 4 second ISR. It does not t...