User Activity

I’m using a VL53L5CXV0DH/1 sensor in my current setup (see pictures). The goal is to detect a ball rolling between the sensor and the background. The red box is about 12cm apart.The settings is 4x4 for speed, i also noticed that 60 is not the highest...
The past few days I have encountered erratic behavior where this message often appears when trying to debug a board:"Launch Terminated:The ELF file does not contain any .text section. Either manually enter the offset for the ELF file in the launch co...
Hi,We have a STM32L031F6 which is used as an RTC. A weird phenomenon is occurring: when the controller goes to sleep, it only uses 2µA, but after 2 minutes and 40 seconds, it starts consuming 50 to 100µA, depending on the hardware board used. There i...
Hi,I need a DMA setup for 4 separate UARTs in an STM32G473 controller. The idea is to always be able to receive data through rxDMA, and only invoke txDMA when sending data. The data that I receive changes in size, is between 20 and 300 bytes, starts ...
Hello,I'm currently working with a custom board designed to read digital values from an accelerometer, specifically from the OUT_X, OUT_Y, and OUT_Z registers. However, I've encountered an issue: despite the accelerometer being physically stable, I a...
Kudos from