cancel
Showing results for 
Search instead for 
Did you mean: 

SPWF04S File print issue

tabekb
Associate III
Posted on June 06, 2017 at 09:51

Hi!

I am using the SPWF04S module configured in MiniAP mode. I've created a file in RAM memory using the AT+S.FSC command.

I am reading the file using the AT+S.FSP command. After about 450-500 successfully readings, the module responds with Low Memory and resets itself (watchdog) after 20 seconds. Sometimes the respond is 'WIND:8:Hard Fault:ConUart:0002b290:20030000:07fd5003:08023588:47938cc4:fb3f49b6:080bb3e0:21000000' instead of Low Memory.

The same happens if I am creating the file using POST messages to the module. In this case I have the following steps:

1. I send this from client PC: curl -i -X POST -H 'Content-type: multipart/form-data' -F 'data=@FileSetX' 172.10.20.1

2. I read the module using 'AT+S.FSP=FileSetX,,'. The content of the file are read correctly.

3. Repeat 1 and 2. After about 400-500 success, the module is blocked (Low Memory / Hard Fault or maybe something else...)

Thanks.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on June 08, 2017 at 14:55

Thanks Tarek, bug solved!

Fix will be part of FW1.1.0

View solution in original post

3 REPLIES 3
Gerardo GALLUCCI
ST Employee
Posted on June 06, 2017 at 20:28

Hi,

please attach here content of AT+S.GCFG command. RAM disk is static, so, cannot use more than that amount of RAM...

Thanks for 500 tests

Ciao

jerry

tabekb
Associate III
Posted on June 07, 2017 at 08:21

Hi!

Probably I was not clear enough. In the first case, I am sending AT+S.FSC command to create a file only ONCE. After that I am reading that file every second. After about 500 readings the issue appear. This should not be a RAM size problem, I am just reading a file containing 5 characters... This is a real situation, reading a file how many time you want should not be limited.

My purpose with 500 tests was to test my application not the module, but I found this issue on the module.

Here follows the AT+S.GCFG:

AT-S.List

AT-S.Var:nv_manuf=ST

AT-S.Var:nv_model=SPWF04SA

AT-S.Var:nv_serial=0317<06103

AT-S.Var:nv_wifi_macaddr=00:80:E1:BD:D5:40

AT-S.Var:standby_time=10

AT-S.Var:standby_enabled=0

AT-S.Var:sleep_enabled=0

AT-S.Var:etf_mode=0

AT-S.Var:blink_led=1

AT-S.Var:ext_volume=3

AT-S.Var:aes128_key=00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

AT-S.Var:user_desc=xxx

AT-S.Var:python_script=3:/uPython_test.py

AT-S.Var:python_memsize=32

AT-S.Var:console_enabled=1

AT-S.Var:console_speed=115200

AT-S.Var:console_hwfc=0

AT-S.Var:console_echo=0

AT-S.Var:console_errs=2

AT-S.Var:console_winds=2

AT-S.Var:console_verbose=1

AT-S.Var:console_repeater=0x21

AT-S.Var:console_delimiter=0x2C

AT-S.Var:console_wind_off_low=0x00000000

AT-S.Var:console_wind_off_medium=0x00000000

AT-S.Var:console_wind_off_high=0x00000000

AT-S.Var:wifi_tx_msdu_lifetime=0

AT-S.Var:wifi_rx_msdu_lifetime=0

AT-S.Var:wifi_operational_mode=0x00000011

AT-S.Var:wifi_beacon_wakeup=1

AT-S.Var:wifi_beacon_interval=100

AT-S.Var:wifi_listen_interval=0

AT-S.Var:wifi_rts_threshold=3000

AT-S.Var:wifi_ssid=45:4C:45:4B:54:52:41:5F:44:45:46:41:55:4C:54:5F:41:50:5F:42:44:44:35:34:30:00:00:00:00:00:00:00

AT-S.Var:wifi_ssid_len=25

AT-S.Var:wifi_txfail_thresh=5

AT-S.Var:wifi_dtim_period=1

AT-S.Var:wifi_add_tim_ie=0

AT-S.Var:wifi_region=1

AT-S.Var:wifi_ht_mode=1

AT-S.Var:wifi_channelnum=6

AT-S.Var:wifi_opr_rate_mask=0x003FFFCF

AT-S.Var:wifi_bas_rate_mask=0x0000000F

AT-S.Var:wifi_mode=3

AT-S.Var:wifi_auth_type=0

AT-S.Var:wifi_atim_window=0

AT-S.Var:wifi_powersave=0

AT-S.Var:wifi_tx_power=18

AT-S.Var:wifi_rssi_thresh=0

AT-S.Var:wifi_rssi_hyst=0

AT-S.Var:wifi_ap_idle_timeout=120

AT-S.Var:wifi_beacon_loss_thresh=10

AT-S.Var:wifi_priv_mode=0

AT-S.Var:wifi_wep_keys[0]=31:32:33:34:35:00:00:00:00:00:00:00:00:00:00:00

AT-S.Var:wifi_wep_keys[1]=00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

AT-S.Var:wifi_wep_keys[2]=00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

AT-S.Var:wifi_wep_keys[3]=00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

AT-S.Var:wifi_wep_key_lens=05:00:00:00

AT-S.Var:wifi_wep_default_key=0

AT-S.Var:wifi_wpa_psk_raw=00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

AT-S.Var:wifi_wpa_psk_text=

AT-S.Var:wifi_eap_identity=identity

AT-S.Var:

mailto:wifi_eap_anon_identity=anonymous@identity.org

AT-S.Var:wifi_eap_passwd=password

AT-S.Var:wifi_eap_type=0

AT-S.Var:wifi_eap_skip_datechecks=0

AT-S.Var:wifi_wps_walk_time=120

AT-S.Var:wifi_wps_pin=1234567

AT-S.Var:ip_sock_memsize=1

AT-S.Var:ip_sock_threshold=0

AT-S.Var:ip_dhcp_lease_time=120

AT-S.Var:ip_macfilter=00:00:00:00:00:00

AT-S.Var:ip_num_clients=5

AT-S.Var:ip_allow_port_scans=1

AT-S.Var:ip_use_v6=1

AT-S.Var:ip_use_dhcpd=1

AT-S.Var:ip_use_httpd=1

AT-S.Var:ip_use_tftpd=1

AT-S.Var:ip_use_dhcpc=2

AT-S.Var:ip_hostname=DEFAULT_AP_BDD540

AT-S.Var:ip_apdomainname=captiveportal.net

AT-S.Var:ip_apredirect=index.html

AT-S.Var:ip_ipaddr=172.10.20.1

AT-S.Var:ip_netmask=255.255.255.0

AT-S.Var:ip_gw=192.168.0.1

AT-S.Var:ip_dns1=208.67.222.222

AT-S.Var:ip_dns2=208.67.220.220

AT-S.Var:ip_local=0:0:0:0:0:0:0:0

AT-S.Var:ip_dns1v6=0:0:0:0:0:0:0:0

AT-S.Var:ip_dns2v6=0:0:0:0:0:0:0:0

AT-S.Var:ip_dhcp_timeout=20

AT-S.Var:ip_ntp_server1=ptbtime1.ptb.de

AT-S.Var:ip_ntp_server2=ntp0.ipv6.fau.de

AT-S.Var:ip_ntp_refresh=3600

AT-S.Var:ip_ntp_startup=1

AT-S.Var:ip_mdns_domain_name=SPWF04S-Default

AT-S.Var:ip_mdns_device_name_ttl=120

AT-S.Var:ip_mdns_services_name=SPWF04S-WebSrv SPWF04S-TFTPSrv

AT-S.Var:ip_mdns_services_prot=_http._tcp _tftp._udp

AT-S.Var:ip_mdns_services_keys=dev1 dev2

AT-S.Var:ip_mdns_services_vals=number1 number2

AT-S.Var:ip_mdns_services_port=80 69

AT-S.Var:ip_mdns_services_ttl=120 60

AT-S.Var:ip_mdns_startup=01:01

AT-S.OK

Thanks

Posted on June 08, 2017 at 14:55

Thanks Tarek, bug solved!

Fix will be part of FW1.1.0