cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, i have a question....could i use 10 lps22hb on same I2C bus?

FItal
Associate II
 
5 REPLIES 5
Eleon BORLINI
ST Employee

​Hi @FItal​ , you can use max n.2 lps22hb on the same physical lines by setting the SA0 pad (SAD[0] bit in the Slave address) high (Vdd) or low (GND). However, you can of course share the communication lines by using the SPI protocol and lowering the CS when you want to communicate with a specific device. Regards

FItal
Associate II

Thanks for the reply.

best regards,

Francesco

Ozone
Lead III

With "dirty" tricks, one can use 10 or more I2C bus slaves with the same address in one bus.

You can gate the SCL line (or better both SCL and SDA) to the slaves, having only two slaves accessible at the bus on any time (at different addresses, set by SA0 pin).

The effort would be similar to managing /CS lines.

Uwe Bonnes
Principal III

There are also I2C Muxes like the PCA9543.

S.Ma
Principal

Connect each pressure sensor slave address select pin to an individual GPIO of the MCU, and make sure only one of them is high (or low) to talk to the one.

Running out of pins on the MCU? Use an I2C IO Expander.