User Activity

We have built a SOM based on STM32MP157 which has eMMC. There were few configuration files which we installed manually. Now, I want a copy of this final working image so that i can duplicate the same image in other emmc too. Please let me know if are...
I have added all required dependencies that I am able to detect the module and allocate with udev rules as modem_1..4 . I have also added ppp feature, but despite that when i dial, it shows some error as indiscipline and here is a log from /var/log/...
In the recently, for the past few days, I am facing this new issue that, if i compile for my custom som and program, i always get this error. But if I dont do any add-on of packages, I works fine.I even added a simple package like "vim" using IMAGE_I...
When we use the PMIC values from DK2 example.1 . ERROR:  regul ldo3: max value 750 is invalidWARNING: register_pmic:600 failed to register ldo3PANIC at PC : 0x2fff05cb2 Next we tried setting the ldo3 max, min values to 3V and 1.8V and it was working ...