User Activity

I can navigate to that from right click and go to declaration. On converting to C++ it starts to give other issues.
Now the issue concluded to the source of issue. The value of Dtata is 0x38 but its not getting transfered to TFR. Though for other resistors its working fine. The value of TFR always stays 0x00000000.  Since the data is not loaded to Tx FIFO, the com...
/******************** (C) COPYRIGHT 2015 STMicroelectronics ********************* File Name     : GPIO/IOToggle/main.c * Author       : RF Application Team* Version      : V1.1.0* Date        : September-2015* Description    : Code demostrating the G...
Pin connection:ST link ------ BLUENRG232SWDIO SWDIOSWCLK SWCLKGND GND3.3V VCCI have also made IO7 high with 10K resister To HIGH.I am using IC and supporting Circuit. I made PCB with supporting circuit for BLUENRG232 IC . The St link utility is not d...
Kudos from