cancel
Showing results for 
Search instead for 
Did you mean: 

I cant connect toBLUENRG 232 IC to BLUENRG ST link utility , Target not connected.

pankajauengg
Associate II

Pin connection:

ST link ------ BLUENRG232

SWDIO SWDIO

SWCLK SWCLK

GND GND

3.3V VCC

I have also made IO7 high with 10K resister To HIGH.

I am using IC and supporting Circuit.

 I made PCB with supporting circuit for BLUENRG232 IC . The St link utility is not detecting the target.

XRCGB32M000F2P26R0Crystal, 32 MHz, SMD, 2mm x 1.6mm, 20 ppm, 5 pF, 20 ppm, XRCGB Series

used oscillator

I had followed " section 3.21 of this Datasheet reports the SWD debug feature."

2 REPLIES 2
pankajauengg
Associate II

Please reply ASAP

pankajauengg
Associate II

I had tried all methods i could but the issue coming is same.