Skip to main content
pankajauengg
Associate II
October 31, 2020
Question

I cant connect toBLUENRG 232 IC to BLUENRG ST link utility , Target not connected.

  • October 31, 2020
  • 2 replies
  • 810 views

Pin connection:

ST link ------ BLUENRG232

SWDIO SWDIO

SWCLK SWCLK

GND GND

3.3V VCC

I have also made IO7 high with 10K resister To HIGH.

I am using IC and supporting Circuit.

 I made PCB with supporting circuit for BLUENRG232 IC . The St link utility is not detecting the target.

XRCGB32M000F2P26R0Crystal, 32 MHz, SMD, 2mm x 1.6mm, 20 ppm, 5 pF, 20 ppm, XRCGB Series

used oscillator

I had followed " section 3.21 of this Datasheet reports the SWD debug feature."

This topic has been closed for replies.

2 replies

pankajauengg
Associate II
October 31, 2020

Please reply ASAP

pankajauengg
Associate II
November 2, 2020

I had tried all methods i could but the issue coming is same.