cancel
Showing results for 
Search instead for 
Did you mean: 

Energy harvesting and LPD: can EH still be active when the ST25 pin is put in LPD mode (the goal is to reduce the whole consumption in EH mode) ?

Brieuc
Associate III
1 ACCEPTED SOLUTION

Accepted Solutions
JL. Lebon
ST Employee

​Hello,

Yes, definitely. EH is completely independent of LPD, so you can have EH power when device in low power mode as well as when device has no VCC.

Best regards.

View solution in original post

2 REPLIES 2
JL. Lebon
ST Employee

​Hello,

Yes, definitely. EH is completely independent of LPD, so you can have EH power when device in low power mode as well as when device has no VCC.

Best regards.

Schuyler
Senior

@JL. Lebon 

Hi,

I need to power the STM32L4 with the energy output from the EH pin. May I ask why my LD3 power point is lit by EH pin, but the MCU does not work normally?