User Activity

Hi, We have developed a product based on the B-U585I-IOT02A platform that includes the wifi part EMW3080(BP) from MXChip.  Our product boardset contains the above MXChip part and we have developed our application code based on the example NetX Duo an...
Hi,I've used many revisions of the CubeMX configuration tool to maintain a Keil uVision project for a product we are developing.  In the past, upon an updated CubeMx version, I have had to re-add my custom files to the project but from then on CubeMx...
I was able to get this working for the L5 with one large circular buffer and interleaved values from the ADC channels 1-4.Given the improved DMA on the U5, I expect that the DMA will not have to generate an interleaved circular buffer of ADC channel ...
Using a STM32L562E-DK. Also using a uLinkPro SW probe.
Kudos from