cancel
Showing results for 
Search instead for 
Did you mean: 

Bluenrg STEVAL-IDB002V1 : Not entering into DFU mode

T.Ratheesh
Associate II
Posted on November 27, 2015 at 15:14

 Hi,

I got a problem while using STEVAL-IDB002V1 eval. kit.

It is not entering into DFU mode if i follow the procedure as per the documentation (because led is not blinking).

Thanks in advance.

Regards ,

Ratheesh T

3 REPLIES 3
Posted on December 01, 2015 at 12:37

Dear Customer,

The STM32L is preprogrammed with a DFU firmware that allows the downloading of a firmware image without the use of a programmer. If an user accidentally erases DFU firmware, he can reprogram it through STLink using the hex image DFU_Bootloader.hex available on DK SW package, firmware folder.

Regards,

GM

T.Ratheesh
Associate II
Posted on December 08, 2015 at 07:17

Hi Marchese.Graziella,

I tried that by using STlink but it is also not working. I have attached the log window which shows some warning

________________

Attachments :

dfu.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I19T&d=%2Fa%2F0X0000000bn9%2FAMh8S54cAc_PFwlp5NqQmIS_eciOdCffiDX0IrXPKpU&asPdf=false
T.Ratheesh
Associate II
Posted on December 10, 2015 at 07:18

Hi,

   Thank you...  Problem Solved

   

   First i tried IAR compiler and ST link debugger for flashing DFU image file (not solved, that was my 2nd post)

 

   After that i tried ST link utility exe (downloader) and ST link debugger                                to flash DFU image it solved  my issue .

  i.e now it can enter into DFU mode