cancel
Showing results for 
Search instead for 
Did you mean: 

BlueNRG TX & RX Buffer size Restriction ?

T.Ratheesh
Associate II
Posted on February 04, 2016 at 13:55

Hi all,

          In BlueNRG chat application, i can able to transfer and receive data if  the packet size was 20 or below. When i change the packet size more than 20 bytes , communication doesn't started. But i need to transfer 35 bytes at a time.

Where i have to change packet size?

Thanks in Advance

Regards

Ratheesh
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on March 09, 2016 at 15:54

Dear Customer,

the BlueNRG chat application is based on Notification, in fact the slave will continuously send notification of 20 bytes to the client and the notification are of 20 bytes.

To transfer more than 20 bytes, you cannot use the notification.

Regards,

GM