User Activity

STEVAL-PTOOL1V1 , is it support 500 rpm to 12000rpm in three wire BLDC Mode. My motor operate 12v or 24V. i Want to Run this BLDC Motor from 500 rpm to 12000rpm at a PWM or Analog Speed Control.i want to also Direction change and Break. this Board h...
Oscilloscope_SignalsGenerator example Not Loading the Kit. i got the Error like Error in final launch sequence:Failed to execute MI command:load E:\\ST\\en.stm32cubeh7_v1-9-0\\STM32Cube_FW_H7_V1.9.0\\Projects\\STM32H735G-DK\\Demonstrations\\Oscillos...
STM32H735 Discovery Example BSP  ** AUDIO LOOPBACK SINGLE-BUFFERING **This example shows how to record and play in loopback an audio stream using DFSDMfor recording and SAI for playing. The data are processed internaly within BSPaudio drivers and ret...
en.x-cube-dspdemo\X-CUBE-DSPDEMO\Projects\STM32F429I-Discovery\STM32F429_DSPDEMO\MDK-ARM When Open and compile error come like below its fresh copy no modification done .how can i resolve that ?compiling BasicMathFunctions.c.....\..\..\..\Dri...