htim5 has been running and I need to zero the count (CNT?).Do I need to stop, de init, init, then start?Also it seems HAL_TIM_OC_Init() is being used with HAL_TIM_Base_Start_IT(() on the same timer, TIM5. It is used to to generate interrupts with a p...