cancel
Showing results for 
Search instead for 
Did you mean: 

ST25R3911B , can it write tags also?

JPehl.1
Associate III

Can ST25R3911B write on tags? Or it is only a reader?

Regards.

1 ACCEPTED SOLUTION

Accepted Solutions
Ulysses HERNIOSUS
ST Employee

Hi JPehl.1,

yes all the NFC readers (actually readers/writers, but people including myself are lazy and omit the "/writers") can exchange arbitrary NFC frames. Whether the frame causes a read operation or write operation on the tag or something completely else is up to the tag itself.

Regards, Ulysses

View solution in original post

2 REPLIES 2
Ulysses HERNIOSUS
ST Employee

Hi JPehl.1,

yes all the NFC readers (actually readers/writers, but people including myself are lazy and omit the "/writers") can exchange arbitrary NFC frames. Whether the frame causes a read operation or write operation on the tag or something completely else is up to the tag itself.

Regards, Ulysses

Thanks very much, solved.