Skip to main content
Machilus
Associate III
November 20, 2020
Solved

How to include TPM2 package when making "Eco system V2.1.0" distribution?

  • November 20, 2020
  • 3 replies
  • 1853 views

Hi ST

I enabled DISTRO_FEATURES_append = "tpm2" in the file ".../layers/meta-st/meta-st-openstlinux/conf/distro/include/openstlinux.inc" as described in the ST Wiki.

When building with "st-image-weston" I get the following error message:

ERROR: Nothing RPROVIDES 'packagegroup-security-tpm2' (but /home/stm32mp1/Work/Ecosystem-V2.1.0/201119_DVT/layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bb RDEPENDS on or otherwise requires it)

NOTE: Runtime target 'packagegroup-security-tpm2' is unbuildable, removing...

Missing or unbuildable dependency chain was: ['packagegroup-security-tpm2']

ERROR: Required build target 'st-image-weston' has no buildable providers.

Missing or unbuildable dependency chain was: ['st-image-weston', 'packagegroup-security-tpm2']

"... / layers / meta-st / meta-st-openstlinux / recipes-st / images / st-image-weston.bb" of the contents of the file "$ {@ bb.utils.contains ('COMBINED_FEATURES', ' tpm2','packagegroup-security-tpm2','', d)} \"There seems to be a package dependency error.

Is there a workaround?

If you build without DISTRO_FEATURES_append = "tpm2" enabled, you cannot use commands like "tpm2_createprimary".

I would appreciate if you can tell me how to fix it.

Thanks and regards

Machilus

This topic has been closed for replies.
Best answer by ArmandG

Hi @Machilus​ ,

You probably did not add the tpm2 recipes to your distribution. Only enabling it is not enough.

To add it, please enter the following commands:

PC $>cd [your STM32MP1 Distribution path]/layers/meta-st

PC $>git clone https://github.com/STMicroelectronics/meta-st-stm32mpu-app-aws.git

And then bitbake again the image.

Armand

3 replies

ArmandG
ArmandGBest answer
ST Employee
November 20, 2020

Hi @Machilus​ ,

You probably did not add the tpm2 recipes to your distribution. Only enabling it is not enough.

To add it, please enter the following commands:

PC $>cd [your STM32MP1 Distribution path]/layers/meta-st

PC $>git clone https://github.com/STMicroelectronics/meta-st-stm32mpu-app-aws.git

And then bitbake again the image.

Armand

Machilus
MachilusAuthor
Associate III
November 23, 2020

Hi ArmandG (ST Employee)

Thank you for answer

I solved the problem in a different way.

I applied the "meta-security" layer for dunfell from the yocto git site.

Actually, even if I built with bitbake, downloaded it to the custom board, and used the tpm2 related utility, no error occurred.

Is there any problem with this use?

Machilus

KMark.1
Associate
June 12, 2022

@Machilus​  I tried both the solutions but I am still getting the error mentioned by you. Can you please tell me what steps you did.