2020-11-19 11:47 PM
Hi ST
I enabled DISTRO_FEATURES_append = "tpm2" in the file ".../layers/meta-st/meta-st-openstlinux/conf/distro/include/openstlinux.inc" as described in the ST Wiki.
When building with "st-image-weston" I get the following error message:
ERROR: Nothing RPROVIDES 'packagegroup-security-tpm2' (but /home/stm32mp1/Work/Ecosystem-V2.1.0/201119_DVT/layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bb RDEPENDS on or otherwise requires it)
NOTE: Runtime target 'packagegroup-security-tpm2' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['packagegroup-security-tpm2']
ERROR: Required build target 'st-image-weston' has no buildable providers.
Missing or unbuildable dependency chain was: ['st-image-weston', 'packagegroup-security-tpm2']
"... / layers / meta-st / meta-st-openstlinux / recipes-st / images / st-image-weston.bb" of the contents of the file "$ {@ bb.utils.contains ('COMBINED_FEATURES', ' tpm2','packagegroup-security-tpm2','', d)} \"There seems to be a package dependency error.
Is there a workaround?
If you build without DISTRO_FEATURES_append = "tpm2" enabled, you cannot use commands like "tpm2_createprimary".
I would appreciate if you can tell me how to fix it.
Thanks and regards
Machilus
Solved! Go to Solution.
2020-11-20 1:28 AM
Hi @Machilus ,
You probably did not add the tpm2 recipes to your distribution. Only enabling it is not enough.
To add it, please enter the following commands:
PC $>cd [your STM32MP1 Distribution path]/layers/meta-st
PC $>git clone https://github.com/STMicroelectronics/meta-st-stm32mpu-app-aws.git
And then bitbake again the image.
Armand
2020-11-20 1:28 AM
Hi @Machilus ,
You probably did not add the tpm2 recipes to your distribution. Only enabling it is not enough.
To add it, please enter the following commands:
PC $>cd [your STM32MP1 Distribution path]/layers/meta-st
PC $>git clone https://github.com/STMicroelectronics/meta-st-stm32mpu-app-aws.git
And then bitbake again the image.
Armand
2020-11-22 4:42 PM
Hi ArmandG (ST Employee)
Thank you for answer
I solved the problem in a different way.
I applied the "meta-security" layer for dunfell from the yocto git site.
Actually, even if I built with bitbake, downloaded it to the custom board, and used the tpm2 related utility, no error occurred.
Is there any problem with this use?
Machilus
2022-06-12 4:40 AM
@Machilus I tried both the solutions but I am still getting the error mentioned by you. Can you please tell me what steps you did.