This post was originally attached to this old, solved thread:
https://community.st.com/t5/stm32-mcus-products/how-to-reset-counter-value/td-p/175202
Hi,
in my case this technique has some drowback. It seems that using the macro __HAL_TIM_SET_CO...
Hi Community, 1) I have to demodulated a continuous bitstream of 201bit (1ms per bit) sent by a host to my stm32F401RE. Which peripheral would you suggest to use?2) If I have to transmitt and receive custom serial data in half duplex with clock in T...
Hi guys,I really need your help.I'm trying to divide two numbers.. But the result is still 0. Analyzind the disassembling the commands are not those of FPU unit. I enable the FPU in the Properties/MCU Setting.Here the simple code:uint32_t A = __HAL_...
HI, I m trying to send a 16 bit word using SPI HAL to a SPI external interface driver. SPI is configured as:-Transmission master-16bit data TX-MSB first.This driver requires first address of the register and then the content to be received. I created...
Thanks, Regarding 2, I forgot to say that the serial data is custom lenght bitstream of 200bit ( no pause in the bitstream, no stop bit between words etc..).Thanks
Hi all, I have you same issue. I created Firmwares directory and tried to copy bin or folders from F401RE/Applications/IKS01A2 of XCUBE MEMS1 9.6 but I still cannot see any icon in the FW Management tab of unicleo GUI. I have flashed Datalog Extended...
Yes, that's right. I actually don't understand why if i import an example, it is created automatically a folder tree like in the first picture.I mean a subfolder STM32CUDEIDE that is the main forlder of the IDE, is made inside the main example folder...