User Activity

If your VL53L8CX gets past the 'is_alive' function but you cannot get it to run, it might be because you are running on a big-endian machine, and the ST code you downloaded assumes a little-endian machine. Try swapping your vl53l8cx_is_alive function...
An anonymous customer was trying to get the best possible range accuracy with a VL53L5 sensor.  His temperature range was from 25degrees C to 50 degrees. This was his plot with no temp cal.  After calibrating between the ranges he got: These plots ...
I heard that ST has extended the lifetime of the L0, L1 and L3.  Can you tell me what the new dates are and where on the website I can find them?  
Customer asks me how I evaluate where the photons go.
I am checking signal status also for Big obstacle it showing Distance up to 2.1 meter(210Cm) and status is 0, and for small obstacle showing distance up to 1.2 meter(120 cm) and status is zero, it is not useful in outdoor environment , and it Hangs a...