User Activity

Hello,I am trying to calculate the x,y,z coordinates of each points of the VL53L5CX sensor to determine the angle error between a surface and the plan of the sensor.I have two problem with my system :- the resulted error is not symmetrical with one r...
Hello !I'm working on the VL53L5CX sensor with a Nucleo L432KC.Using the ST example, and after succeeded the initialization of the VL53L5CX, the sensor's data are never ready. In the following function, the p_dev->temp_buffer[1:4] are all equals to 0...
Hi ! I'm using the VL53L4CD sensor's example with the Nucleo-L432KC.A first problem I solved was that the VL53L4CD didn't have the adress 0x52 as in the documentation, but 0x29 (this problem has already mentioned in a topic).My current problem is tha...
Kudos from
Kudos given to