Skip to main content
RMasi.19
Associate III
July 22, 2022
Question

PMSM hardware with MCSDK v6

  • July 22, 2022
  • 1 reply
  • 684 views

Hi good day, i have a fanuc AC PMSM 140v, 6NM, 4.6A, 1kw, 2000ppr

i see the tool hardware and think what the follow kit is convenient:

1.- Nucleo G431RB

2.- X-nucleo IHM09M1

3.- STEVAL-IPM30B

but i see MCSDK v6 no support this hardware, then I ask some general questions because i am just starting in ST motor control although i already have some experience in PMSM with other micros.

the configuration of the parameters of the motor Fanuc and the hardware follow still simple for the v6?. is necesary i migrate a some version 5.x and what version ?.

this FOC library can control IPMSM and SPMSM?, how the MCSDK detect or recognize the type of motor?

The field alignment of rotor and stator in the start is made always?, this need UVW channel encoder for alignment field,? why i see servodrivers PMSM what no make this movement initial of alignmet field

Thanks

This topic has been closed for replies.

1 reply

GMA
ST Technical Moderator
July 27, 2022

Hello,

  • For the motor characteristics, you have to use ST provided tool "ST motor profiler". I-PMSM/SM-PMSM has to be set at this step.
  • You can use 5.Y.4 version, selecting G431+IPM30, IHM09 will be automatically added.
  • Alignment is needed if a quadrature encoder is used.
  • Incremental encoder needs zero reference, absolute encoder (e.g.) not....

Best regards.

GMA

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA