User Activity

Hi everyone,I'm encountering an issue with the STM32 Device Configuration Tool: it doesn't properly generate the global interrupt handler function for one of the UARTs in my project: The generated interrupt handlers for USART1 and USART2 include call...
Hello everyone!I'm asking for your help with the following: I have a board equipped with an STM32L151 processor, with which I use an STM32 ISM330DHCX IMU via I2C. The ODR is set to 52Hz for both the gyroscope and the accelerometer, and I request an a...
Hi everyone!I have to implement a dual bootloader system on different stm32 microcontrollers in STM32cube ide, and I have some questions…The idea is the following:There is a “pre-bootloader�? at the beginning of the flash. When it starts, it gets som...
Kudos given to