cancel
Showing results for 
Search instead for 
Did you mean: 

When I try to generate user code through CubeMX 6.4.0, the program hangs. If I try to update user code from a demo project, the program doesn't hang. Why?

MBale.1
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
TDK
Super User

There is not enough detail in this question to provide an informed response. Probably one program has bugs while the other may not. Diff the source files.

If you feel a post has answered your question, please click "Accept as Solution".
Sara BEN HADJ YAHYA
ST Employee

Hello @MBale.1​ ,

Thanks for your feedback,

Could you please share your .ioc file and specify which demo are you using?

Thanks,

Sara.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
MBale.1
Associate II

The demo I am using is called "Six-Step Sensorless and Voltage Mode on a STEVAL-SPIN3204+Shinano LA052-800"

Sara BEN HADJ YAHYA
ST Employee

Hello @MBale.1​ ,

Could you please provide us with more details, does your code disappear when you regenerate your code, is that your issue?

Sara.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
MBale.1
Associate II

Here are my issues:

  1. When I create a new project and press "Generate", CubeMX gets stuck and does nothing.
  2. When I try to open any of the demo projects and press "Update", CubeMX also gets stuck and does nothing

This is using ST Motor Control Workbench 5.Y.3 with CubeMX 6.4.0