User Activity

Hello,I am experiencing an interesting problem on the STM32F303VET:UART1 is used to receive and transmit messages (460800 Baud), DMA1 Channel 4 is used for memory to UART TX buffer transfer, DMA1 Channel 5 for UART RX buffer to memory transfer.Under ...
When changing the timebase source in CubeIDE from Systick to any peripheral timer (TIM6 in my test case), the timer is set up in HAL_InitTick() called from the HAL_Init() function, which is the first function that is called in main().HAL_InitTick() u...
I would like to share a bug I encountered and how to fix it:I am using an STM32L151, the goal is to set it into SLEEP mode and wake it up using a UART receive interrupt while debugging. All configurations to pins, registers and interrupts are made co...
CubeMX does no longer create the TIM1_UP_TIM10_IRQHandler in the stm32f4xx_it.c file after the timebase source have been changed to any timer and System tick timer 'Generate IRQ handler' and 'Call HAL handler' code generation has been disabled in NVI...
Kudos from