Skip to main content
Altamash Abdul Rahim
Associate III
June 29, 2022
Question

Bluenrg-2(M2SP) module advertisement failure after a while.

  • June 29, 2022
  • 2 replies
  • 858 views

@Winfred LU​ 

Hello i have been using bluenrg-2 module for quite some time and i have noticed that after working well for the 2-4 days continuously sometimes the module does not show up in scan request i.e. it does not advertises. I'm sure the while there is an advertisement issue the device is working well because that i can verify via the device logs which are generated by the device application code.

Has anyone else faced this issue if so please help me out.

Thanks and Regards

    This topic has been closed for replies.

    2 replies

    Altamash Abdul Rahim
    Associate III
    July 15, 2022

    @Winfred LU​  ??

    Winfred LU
    ST Employee
    August 12, 2022

    Hi Altamash,

    Some comments for your reference to further investigate.

    What are the tasks for the module during the 2-4 days continuously working? Could you narrow down to a short period before the issue occurs?

    When issue occurs, does the module receive any packet correctly?

    If you perform a software reset through the application processor, would the module work around?

    Is is possible to connect through SWD to understand if the firmware is still running?

    Is the module always in sleep when advertising is stopped? You can verify it by checking VDD1V2. If it is always low it is in sleep.

    Is the stack raising hci_hardware_error_event() sometimes?

    What is the value of the HS_STARTUP_TIME?

    Best Regards,

    Winfred