2022-09-20 6:19 PM
Section 6.4.4 of RM0433 is the only place I could find that says what to do with VBAT rail when not using a battery. It says the following:
If no external battery is used in the application, it is recommended to connect VBAT externally to VDD through a 100 nF external ceramic capacitor.
Does it actually mean "through"? That wording implies this:
 
...but I don't see how that make sense.
Does anyone else read it differently?
Solved! Go to Solution.
2022-09-21 2:46 AM
Welcome, @NAbun.1, to the community!
This is indeed misleading and means that you should connect VBAT to VDD and from that connection connect the capacitor to GND.
Does it answer your question?
Regards
/Peter
2022-09-21 2:46 AM
Welcome, @NAbun.1, to the community!
This is indeed misleading and means that you should connect VBAT to VDD and from that connection connect the capacitor to GND.
Does it answer your question?
Regards
/Peter
2022-09-22 11:12 AM
Thank you for the warm welcome! I am just getting into the STM32 micros and have a lot to learn.
I believe you did answer my question, thanks!
2022-09-23 12:49 AM
Great! Wish you much success working with the STM32!
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Regards
/Peter
2022-09-23 11:08 AM
Of course, my apologies. It is done now!