How to change endian in a 16bit SPI transmission?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-04-22 11:38 PM
HI,
I m trying to send a 16 bit word using SPI HAL to a SPI external interface driver.
SPI is configured as:
-Transmission master
-16bit data TX
-MSB first.
This driver requires first address of the register and then the content to be received.
I created a struct:
typedef struct
{
uint8_t regAddr;
uint8_t regData;
} SDR_TypeDef;
and then I define a variable with the contents:
SDR_TypeDef decodeMode_Reg={0};
decodeMode_Reg.regAddr = DECODE_MODE_ADDR; // 0x9
decodeMode_Reg.regData = 0b10001010; //0x8A
and then transmission by HAL:
HAL_SPI_Transmit(&hspi, (uint8_t*) &decodeMode_Reg, 1, HAL_MAX_DELAY);
On the scope I have a reverse endian transmission: 8A09 instead of 098A.
Any ideas?
I would like to let the struct in this way, without reversing the order of registers, since it fits better the definition of the register of the receiver driver datasheet. Some ideas?
Thanks
- Labels:
-
SPI
-
STM32Cube MCU Packages
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-04-22 11:42 PM
Either use 8-bit frame size or declare the structure as:
typedef struct
{
uint8_t regData;
uint8_t regAddr;
} SDR_TypeDef;