2022-12-14 5:09 AM
Here I used BLUENRG-LP SoC with ASM330LHH. We have the same schematic design in steval-IBD11V2A, like the first image. The second one is our schematic design.
My I2C configuration init function is like:
/**
* @brief Configures the I2C interface used for the sensor ASM330LHH.
* @param None
* @retval None
*/
void BSP_I2C_Init(void)
{
/* Initialize the GPIOs associated to the I2C port */
BSP_I2C_DATA_GPIO_CLK_ENABLE();
LL_GPIO_SetPinMode(BSP_I2C_DATA_GPIO_PORT, BSP_I2C_DATA_PIN, LL_GPIO_MODE_ALTERNATE);
LL_GPIO_SetPinSpeed(BSP_I2C_DATA_GPIO_PORT, BSP_I2C_DATA_PIN, LL_GPIO_SPEED_FREQ_HIGH);
LL_GPIO_SetPinOutputType(BSP_I2C_DATA_GPIO_PORT, BSP_I2C_DATA_PIN, LL_GPIO_OUTPUT_OPENDRAIN);
LL_GPIO_SetPinPull(BSP_I2C_DATA_GPIO_PORT, BSP_I2C_DATA_PIN, BSP_I2C_DATA_GPIO_PULL);
BSP_I2C_DATA_GPIO_AF();
BSP_I2C_CLK_GPIO_CLK_ENABLE();
LL_GPIO_SetPinMode(BSP_I2C_CLK_GPIO_PORT, BSP_I2C_CLK_PIN, LL_GPIO_MODE_ALTERNATE);
LL_GPIO_SetPinSpeed(BSP_I2C_CLK_GPIO_PORT, BSP_I2C_CLK_PIN, LL_GPIO_SPEED_FREQ_HIGH);
LL_GPIO_SetPinOutputType(BSP_I2C_CLK_GPIO_PORT, BSP_I2C_CLK_PIN, LL_GPIO_OUTPUT_OPENDRAIN);
LL_GPIO_SetPinPull(BSP_I2C_CLK_GPIO_PORT, BSP_I2C_CLK_PIN, BSP_I2C_CLK_GPIO_PULL);
BSP_I2C_CLK_GPIO_AF();
/* Initialize the I2C clock */
BSP_I2C_CLK_ENABLE();
LL_I2C_Disable(BSP_I2C);
/* Configure the SDA setup, hold time and the SCL high, low period
* For Fast-mode 400 kHz, PRESC | 0h | SCLDEL | SDADEL | SCLH | SCLL
* 1h | 0h | 3h | 2h | 03h | 09h
*/
__IO uint32_t timing = __LL_I2C_CONVERT_TIMINGS(0x03, 0x04, 0x02, 0xF, 0x13);
printf("timing in BSP_I2C_Init: %#x, \r\n", timing);
LL_I2C_SetTiming(BSP_I2C, timing);
// LL_I2C_SetTiming(BSP_I2C, 0x10320309);
// LL_I2C_SetTiming(BSP_I2C, 0x00200204);
/* Enable Clock stretching */
LL_I2C_EnableClockStretching(BSP_I2C);
/* Enable Peripheral in I2C mode */
LL_I2C_SetMode(BSP_I2C, LL_I2C_MODE_I2C);
/* Enable the I2C peripheral */
LL_I2C_Enable(BSP_I2C);
/* Enable I2C transfer complete/error interrupts:
* - Enable Receive Interrupt
* - Enable Not acknowledge received interrupt
* - Enable Error interrupts
* - Enable Stop interrupt
*/
// LL_I2C_EnableIT_TX(BSP_I2C);
// LL_I2C_EnableIT_RX(BSP_I2C);
// LL_I2C_EnableIT_TC(BSP_I2C);
// LL_I2C_EnableIT_NACK(BSP_I2C);
// LL_I2C_EnableIT_ERR(BSP_I2C);
// LL_I2C_EnableIT_STOP(BSP_I2C);
}
When I tried to use API, I can't get whoamI ID. The result is 0.
#ifdef TEST_INERTIAL_SENSOR
/* Initialize the handle of the LPS22HH driver */
inertialHandle.write_reg = BSP_I2C_Write;
inertialHandle.read_reg = BSP_I2C_Read;
/* Inizialize the I2C */
BSP_I2C_Init();
LL_mDelay(1000);
/* Wait sensor boot time */
LL_mDelay(BOOT_TIME);
/* Check device ID */
uint8_t result;
asm330lhh_status_reg_t reg;
result = asm330lhh_device_id_get(&inertialHandle, &whoamI);
result = asm330lhh_status_reg_get(&inertialHandle,®);
printf("whoamI: %d, \r\n", whoamI);
printf("ID: %d, \r\n", ASM330LHH_ID);
printf("result: %d, \r\n", result);
I don't know what's the problem. My guess is the set timing is wrong. Because I tried many times with different value.
2023-01-22 1:20 PM
I have a similar problem. I am using HAL libraries instead of LL. Whit SPI I was able to read WHO_AM_I and temperature but was unable to get accelerometer and gyro data.
2023-01-28 4:18 PM
Finally, I figured out where the problem is. I changed the codes: (in both BSP_I2C_Write and BSP_I2C_Read)
From:
LL_I2C_TransmitData8(BSP_I2C, (Reg | 0x80));
To:
LL_I2C_TransmitData8(BSP_I2C, Reg);
Here raised a new question: Why we sometimes need Reg | 0x80, sometimes not?