Question
Nucleo-L412 Programming Error
Hi. I have Nucleo-L412 programming error with Keil. I can program Nucleo F401, F411 and F407 discovery board without error. But I can not load the program to the L412 board. I had had "No ST Link Detected error" but then I solved this problem on Keil "Debug-(Add) Flash Download" preferences. Now it looks like I can download the code to the Nucleo but It does not work even Blinky program. JP1 pin is On.