User Activity

I have an RS585 1/2 duplex transceiver hooked to USART2 configured for hardware flow control (RS485) on an STM32L412 micro.Is it possible to program a virgin part using the STM32CubeProgrammer, and to later do a firmware update over this comm channel...
I'm using the STM32H743 and the it will not allow me to choose fast mode for a 400kHz clock speed. Is that a bug in the IDE?
I have VBUS sensing enabled and when I step through the call to HAL_PWREx_EnableUSBVoltageDetector(), you'd expect a difference in the bit states in the OTG_HS_GCCFG register but there is no difference whether the cable is plugged in or not.I find it...
I've tried 10 or more times now to get around this problem.I'm choosing the STM32F413RGtx for the uC in STM32CubeIDE new STM32 project,I go to generate code from the embedded CubeMX screen and it always tries to download that stm32cube_fw_f4_v1240.zi...