User Activity

Since the poorly soldered microUSB connector on the eval board broke off, I fixed and wired USB-A connector. If the board is then connected to PC, STM DFU device appears in Device Manager and appropriate driver could be installed so I suppose that th...
WiSE Studio does not connect to Segger J-Link, although Atollic TrueStudio and J-Link Commander do. Could it be in a different driver? Why different?I am evaluating the BlueNRG-2 eval board that is working under TrueStudio (that cannot compile an SDK...
I imported the BLE Beacon example fromC:\ST\BlueNRG-1_2 DK 3.2.2\Project\BLE_Examples\BLE_Beacon\WiSE-Studio\STEVAL-IDB008V1Min Atollic TrueStudio 9.3.0 ("Existing Projects into Workspace")but after clicking the 'Build' button, the console prints:***...
I downloaded the BLE Beacon / Relase example from BlueNRG-1_2 DK 3.2.2 into eval board STEVAL-IDB008V1M by BlueNRG-2 Navigator.I do not see this BlueNRG BT device in laptop although a serial console on VCP shows that all functions passed with success...