2022-07-22 3:02 AM
I downloaded the BLE Beacon / Relase example from BlueNRG-1_2 DK 3.2.2 into eval board STEVAL-IDB008V1M by BlueNRG-2 Navigator.
I do not see this BlueNRG BT device in laptop although a serial console on VCP shows that all functions passed with success.
aci_gatt_init() --> SUCCESS
aci_gap_init() --> SUCCESS
hci_le_set_scan_resp_data() --> SUCCESS
aci_gap_set_discoverable() --> SUCCESS
hci_le_set_advertising_data() --> SUCCESS
BlueNRG-1,2 BLE Beacon Application (version: 1.1.0)
However, an Android smartphone shows an available device 02:80:E1:00:00:00, but pairing does not process.
Any opinion?
2022-08-01 10:49 AM
Pairing in BLE is not used (at all or only in a standard way?) so BT devices do not show advertising BLE devices
I should use a BLE scanner on my smartphone.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.