cancel
Showing results for 
Search instead for 
Did you mean: 

SBSFU & Touchgfx ->Firmware signature check failure.

JChou.1
Associate III

Hi all,

SBSFU ported to many custom boards and in projects, and is working as expected.

But in a project with Touchgfx throwing error "error was: Firmware signature check failure." on Installing update FW from download area.

As it is working for other projects without Touchgfx,

I'm really clueless where to look?

I'll appreciate for any info.

With regards

Jitu

2 REPLIES 2
Bubbles
ST Employee

Hi @JChou.1​ ,

what particular MCU are you using? What development tools?

Sometimes when there is code in ITCM or CCM memory range, the prepareimage.py is confused about it and creates incorrect FW image. Or it could be something else, please provide details.

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

JChou.1
Associate III

Hi Jhoud,

MCU : STM32F446

Development tool: STM32CubeIDE 1.5.0

SBSFU type: 2_image

As the complete image (.bin generated by prepareimage.py ) runs and only the .sfb on fw update causing error.

With regards

Jitu