cancel
Showing results for 
Search instead for 
Did you mean: 

Changes require to display graphic on the vertical drawing pixel( vertical bytes orientation e.g. display driver SSD1309 etc.).

JChou.1
Associate III

Hi,

I have successfully implemented a complete graphic to display some system related parameter on a monochrome OLED Display with display driver SSD1322, which is a horizontal drawing pixel, however porting the same code to a monochrome OLED Display with display driver SSD1309 result in a gibberish (see the pics), it supposed to look like pics 1 & 2.

Is there any changes or function build in TOUCHGFX to transform the horizontal byte orientation to vertical byte orientation ?

ref:

Vertical byte orientation e.g. (of a square block):

uint8_t Vdata[16] = {0xF0, 0x10, 0x10, 0x90, 0x90, 0x10, 0x10, 0xF0,

            0x0F, 0x08, 0x08, 0x09, 0x09, 0x08, 0x08, 0x0F};

Horizontal byte orientation e.g. (of a square block):

uint8_t Hdata[16] = {0x00, 0x00, 0x00, 0x00, 0xFF, 0x81, 0x81, 0x99,

            0x99, 0x81, 0x81, 0xFF, 0x00, 0x00, 0x00, 0x00};

I'll appreciate for nay help.

thanks

Jitu

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0